System Settings
| Phase Naming Convention | Select the naming convention for phases: 123, ABC, or UVW. The selected naming convention for phases will be used throughout this application display. |
| Voltage Offset Adjustment | Set a voltage offset for both the Output Terminal and the Sense Terminal for each phase. Output Terminal – Voltage offset when the sensing function is not in use. Sense Terminal – Voltage offset when the sensing function is in use. |